The RECOM group in Gmunden, Austria, has built a campus-like headquarters site with a total of three thousand square metres of floor space in a bid to intensify the company’s commitment to the electrical power supply. In addition to a modern logistics centre and new management facilities, RECOM has placed special focus on its labs, extending the R&D, testing, investigation and quality assurance labs by a state-of-the-art EMC lab; this comes as a substantial boost to the company’s capabilities in the high-frequency range serving Austria and southern Germany. The 3m-SAC (semi-anechoic chamber) equipped by Rohde & Schwarz will see standard-compliant measurements performed at a frequency range of 30 MHz to 3 GHz according to CISPR22. The SAC features an automated measurement procedure on test pieces at up to one metre in diameter, and the computer-controlled turntable and near-field probes allow fully automatic determination of critical interference sources in each test piece.