Energy Harvesting

“Energy harvesting” means collecting energy from an external ambient energy source, such as light, heat, movement or EM fields and storing it as electrical energy in a battery or capacitor for later use. The principle is that a continuous supply of low-level energy can be harvested to provide a short-term higher energy output. The stored energy is typically used to supply power to low-power wireless electronic devices, such as microprocessors, sensors, or network communications.

The electromagnetic spectrum of UV and visible light

Fig. 1: The electromagnetic spectrum of UV and visible light

The most common ambient energy sources are:

Photovoltaic

Solar cells can generate useful amounts of power by absorbing photons of light even at indoor locations. The open-circuit DC output voltage of a PV cell is around 500V–800mV at 100 Lux, but higher voltages can be generated by wiring several cells in series, using larger cells or by exposing the cells to stronger light. If heavily loaded, the output voltage drops significantly, so the optimum loading (maximum power point) should be constantly adjusted (tracked) to compensate for any changes in light intensity.

Thermoelectric

If there is a temperature gradient across two dissimilar conductors, then they will generate an electric current between them (this is known as the Seebeck effect). Thermoelectric generators (TEGs) use this effect to convert ambient heat into electricity using semiconductor junctions to generating usable amounts of DC power. The DC power increases in proportion with the temperature difference between the hot and cold junctions and the surface area of the generator.

Vibration

The most common vibrational energy harvesters use a spring-loaded mass that moves a magnet within fixed coils to generate AC electric power. If the mass-spring system is tuned to be resonant with the main frequency of the vibration, then it can produce significant amounts of power.

Mass-Flow

Moving liquids or gases will spin a small turbine to produce electricity. Such micro-turbines can be placed in air-conditioning ducts, water pipes or on the external surface of vehicles to generate AC power from the flow of air or water generated by the movement of the vehicle. Vortex-shedding is an alternative mass-flow energy harvesting method that has no rotating parts (see piezoelectric).

Piezoelectric

Converts mechanical strain into a high voltage, low current output that can be used as an energy source for a harvester. For example, a piezoelectric base is often used with a vibrating vortex-shedding wand to convert the oscillations into an AC voltage.

Electromagnetic

A device that collects and uses electromagnetic radiation (electric fields, Wi-Fi signals, radio waves) using an antenna to generate very low power (typically µW). It is used indoors. However, high power can be generated if directed microwave beams are used as the source at outdoor locations.

Electronic Components of an energy harvesting system:

Boost converter

Most ambient energy sources are capable of delivering output voltage that is too low to be used directly. So the first stage of a harvesting system is a DC/DC boost converter. The boost converter raises the low input voltage to a higher voltage that can then be used to charge a small battery or a supercapacitor. For example, the REH harvester accepts input voltages starting from 0.05 VDC and boosts the voltage up to either 4.12 VDC to charge a rechargeable battery or 4.50 VDC to charge a two-cell supercapacitor (pin selectable).

System controller

The system controller controls the charging and discharging of the energy storage elements to make sure that they are not over-charged or over-discharged. It also generates status signals and a warning signal of imminent power failure if the load drains the storage element completely. In the case of the REH harvester, the controller also contains a battery backup switch to alternately supply the load from a primary-cell battery if there is not enough ambient energy available (For example, for a photovoltaic cell source at night).

Buck converter

The voltage stored in the storage element (battery or supercapacitor) is variable and not short circuit protected. The buck converter efficiently drops this unregulated supply down to a stable, fixed-voltage output, which is short-circuit protected. The REH harvester contains two independent regulated buck converters to supply 3.3 VDC and 1.8 VDC to power the application.
block diagram
  Series Main Vout (V) Vin (V) Package Style
1 AC/DC, 4 W, Single Output RAC04NE-K/277 Series
Focus 신규
12, 15, 24, 5, 9 85 - 305 Encapsulated 1.45"x0.94", Encapsulated 1.48"x0.97" (IP65)
2 DC/DC, Dual Output, SMD (pinless) REH Series
1.71 to 3.47 / 1.8 0.05 - 5 25 pad LGA
3 DC/DC, Dual Output REH-3.31.8-EVM-1 Series
1.71 to 3.47 / 1.8 0.05 - 5 Open Frame

...didn't find what you were looking for?

Use our parametric search or find a sales contact near you.

제품 검색

주요 사양 기준에 따라 제품을 찾아보세요.

영업 지원

가까운 문의처를 찾아보시기 바랍니다.