Unregulated or Regulated Converters
RECOM offers isolated DC/DC converters in both regulated and unregulated versions. The choice between the two depends on the specific application. If the supply voltage is regulated and the load remains relatively constant, an unregulated DC/DC converter may offer the ideal solution. This is because an unregulated DC/DC converter still offers voltage level conversion, galvanic isolation, and short-circuit protection (/P versions) while also being significantly cheaper than a regulated DC/DC converter.
Conversely, if the supply voltage or load is not stable, a regulated converter is needed since it is designed to maintain the output voltage at the desired value despite input voltage or load variations. A regulated DC/DC converter will maintain a fixed output voltage if the input voltage varies (for example, if it is battery-powered) or if the load is variable, including no-load conditions.
In some low-power designs, a semi-regulated solution offers the best compromise. An unregulated converter incorporating a linear low-dropout (LDO) voltage regulator on the secondary side of the transformer maintains the output at the desired value, irrespective of load conditions. The tradeoff is that the additional regulation stage reduces the overall efficiency and increases the cost compared to an unregulated converter, although it has the advantage that if the load is suddenly removed, the output voltage remains stable and the converter continues to be short-circuit protected.
Here are some of the many areas where these versatile devices are used. Both regulated and unregulated converters are included, depending on the application.
Conversely, if the supply voltage or load is not stable, a regulated converter is needed since it is designed to maintain the output voltage at the desired value despite input voltage or load variations. A regulated DC/DC converter will maintain a fixed output voltage if the input voltage varies (for example, if it is battery-powered) or if the load is variable, including no-load conditions.
In some low-power designs, a semi-regulated solution offers the best compromise. An unregulated converter incorporating a linear low-dropout (LDO) voltage regulator on the secondary side of the transformer maintains the output at the desired value, irrespective of load conditions. The tradeoff is that the additional regulation stage reduces the overall efficiency and increases the cost compared to an unregulated converter, although it has the advantage that if the load is suddenly removed, the output voltage remains stable and the converter continues to be short-circuit protected.
Here are some of the many areas where these versatile devices are used. Both regulated and unregulated converters are included, depending on the application.