Be careful with power density comparisons
The power density specification of an AC/DC converter is a good comparative measure of size as long as the environmental conditions are comparable and realistic - some high-end (read: expensive) modules in custom housings can boast impressive figures of over 100W/cubic inch (6W/cm3), but these often need excessively large or water-cooled heatsinks and sometimes achieve their compact size by omitting large external components such as the input filter and the rectifier electrolytic capacitor. For typical applications where cost and ease of use are important, a realistic comparison is really between modules in industry-standard footprints such as 5” x 3” or 4” x 2”, which are fully integrated without the need for external components.
These AC/DC converters will normally headline their data sheets with the highest possible power output under the most favourable operating conditions. To be fair, there might be many applications that have the optimum AC input voltage and can provide the necessary ambient cooling airflow. In some product datasheets, airflow figures of over 35 m3/hr (20 CFM) are specified for cooling to achieve full rated power, which typically requires a 60mm x 60mm x 25mm axial fan placed directly next to the converter, with access to inlet air at ambient room temperature and a direct route to exhaust the hot air without any obstruction. Figure 1 shows how this is calculated. The fan could easily be a quarter of the size of the power supply in volume, costing several euros and taking a precious 1.5 Watts itself.
Fig. 1: Calculating air flow given power dissipated and target temperature difference
A built-in fan just for the power supply is not always practical and airflow from larger system fans may not be able to provide sufficient localised high flow-rate air, which could anyway be pre-warmed by other hot components, diminishing the cooling effect.
These AC/DC converters will normally headline their data sheets with the highest possible power output under the most favourable operating conditions. To be fair, there might be many applications that have the optimum AC input voltage and can provide the necessary ambient cooling airflow. In some product datasheets, airflow figures of over 35 m3/hr (20 CFM) are specified for cooling to achieve full rated power, which typically requires a 60mm x 60mm x 25mm axial fan placed directly next to the converter, with access to inlet air at ambient room temperature and a direct route to exhaust the hot air without any obstruction. Figure 1 shows how this is calculated. The fan could easily be a quarter of the size of the power supply in volume, costing several euros and taking a precious 1.5 Watts itself.
Fig. 1: Calculating air flow given power dissipated and target temperature difference
A built-in fan just for the power supply is not always practical and airflow from larger system fans may not be able to provide sufficient localised high flow-rate air, which could anyway be pre-warmed by other hot components, diminishing the cooling effect.