Consider a typical efficiency/load graph for a 10W AC/DC power supply (e.g., RAC10-12SK/277).
The efficiency overload graph is quite flat for all loads approximately over 20%, which is good, but at 50% load (5W), the efficiency varies between 77% and 81% depending on the supply voltage (Figure 1, orange line). At 100% load, the efficiency remains constant at 83% irrespective of the input voltage (Figure 1, blue line).
This difference may not seem significant, but 77% efficiency means that 30% of the supplied energy is wasted as heat, while 83% efficiency means only 20% is wasted – a significant reduction in the dissipated power. If the power supply was replaced with an equivalent 5W rated part, say the RAC05-K/277, then the efficiency would be a constant 83%, irrespective of the supply voltage (Figure 2).
The efficiency overload graph is quite flat for all loads approximately over 20%, which is good, but at 50% load (5W), the efficiency varies between 77% and 81% depending on the supply voltage (Figure 1, orange line). At 100% load, the efficiency remains constant at 83% irrespective of the input voltage (Figure 1, blue line).
This difference may not seem significant, but 77% efficiency means that 30% of the supplied energy is wasted as heat, while 83% efficiency means only 20% is wasted – a significant reduction in the dissipated power. If the power supply was replaced with an equivalent 5W rated part, say the RAC05-K/277, then the efficiency would be a constant 83%, irrespective of the supply voltage (Figure 2).