Modified Standard, Semi-Custom, and Full-Custom Power Supply Designs – The RECOM Approach

RECOM 전원 공급장치와 맞춤형 솔루션 표시
RECOM offers over 30,000 standard portfolio DC/DC and AC/DC products, but at times, a non-standard converter is needed. This article explores the difference between modified standard, semi-custom, and full-custom power converters.

One of the reasons RECOM has the broadest power converter portfolio in the industry is the sheer number of variations available within its standard product range. If we take a classic 5W isolated and regulated DC/DC converter in a DIP24 case, such as the REC5 series, the datasheet shows five input and nine output voltage options, including single and dual outputs.

There are three different isolation voltage ratings from 2kV up to 6kV, and three pinning configurations to make it a pin-compatible alternative to competing products, including a version with a remote on-off pin. Additionally, the board mounting pins can be either through-hole or SMT. The case material is available in plastic or metal. Finally, the series comes in either tube or tape-and-reel packaging. Overall, this one DC/DC converter series supports well over two thousand permutations as standard.

Modified Standard Power Converter

변압기, 옵토커플러 및 션트 레귤레이터 회로 다이어그램
Fig. 1: Simplified shunt regulator circuit (in this circuit, Vset would be Vref(1+(R1/R2)) + Voptodiode)
It may seem that all possible customer requests would be covered with such a wide portfolio of catalog products, but occasionally, specific characteristics requested by customers fall outside these standard options. For example, a customer might require different pin lengths (shortened or extended) or a 5.7V output voltage instead of the standard 5V to accommodate an OR-ing diode in the output circuit. Such requests are straightforward to implement and fall under the category of modified standard products.

To understand why a modified output voltage is so simple to achieve, it helps to examine the most common method of regulating output voltage in a DC/DC or AC/DC converter: an output shunt regulator based on a precision programmable reference IC (Figure 1).

During each switching cycle, the output voltage rises until the shunt regulator set voltage, Vset, is exceeded, at which point the optocoupler is energized and the cycle is reset. Despite its simplicity, this circuit accurately regulates output voltage under varying load and line conditions. The switching duty cycle—and therefore the output voltage—is determined by the transformer’s turns ratio, the Vref voltage (typically 1.22V), and the two programming resistors, R1 and R2.

Modifying this converter to deliver 5.7V instead of 5.0V simply requires fitting alternative R1 or R2 values to adjust the programming divider ratio—a straightforward modification that can be implemented at little to no extra cost. Since RECOM operates its own SMD assembly lines, producing a batch of converters with a modified output voltage involves only a change in the production SOP and the laser-printed label.
출력 전압 vs. 부하 그래프
Fig. 2: Example of an unregulated converter voltage tolerance diagram (R1SX series)
We can also optimize the choice of component values to better match the specific requirements of the customer’s end application, rather than relying solely on a standard converter. For example, in an unregulated DC/DC converter, the output voltage is influenced by both the load and input voltage. In most cases, we tune the component values so that the nominal output voltage is achieved at nominal input voltage and 80% load, as illustrated in the output voltage tolerance envelope (Figure 2).

This standard configuration fulfills the most common requirements for the output voltage tolerance for unregulated DC/DC converters, which typically operate at slightly less than full load. The compromise is that the output voltage is lower at full load and higher at low loads. Should a customer demand that the output voltage rise to less than +7% under low load conditions, then we can modify the design to keep the output voltage under, say, +5% by adjusting the component values so that the Vnom voltage is delivered at 70% load instead of 80%, effectively shifting the tolerance envelope downwards. The disadvantage would be a lower output voltage at full load, but this may not matter in this particular application.

However, the amount of output voltage modification that can be achieved by optimising the component values to better match the requirements of the end application is limited. The nominal output voltage depends on the turns ratio of the transformer, so if the required output voltage deviates too far away from the standard, then a modified transformer with an adjusted turns ratio may be needed. This would entail not only a custom transformer part number but also a re-certification of the safety standards. This moves us away from a modified standard converter and into the realm of a semi-custom design.

Semi-Custom Power Converter

The boundary between a semi-custom and a modified standard power converter is not always obvious, so a useful definition is whether safety re-certification is needed. Modifications that affect safety-critical components or separations – such as the transformer construction, the choice of optocoupler or Y-capacitor, or creepage and clearance distances – will almost certainly require a new certification process. However, the safety test reports typically allow a ±10% variation in the output voltage and current ratings to accommodate production tolerances, leaving some scope for flexibility.

The input voltage rating also has at least a ±20% tolerance, and often more. If the required modification stays within these tolerance bands, then safety re-certification may not be necessary. The same applies if the original safety test report lists ‘alternate construction’ options for certain components or potting materials. We have customer applications where silicone potting material is not acceptable, either due to potential outgassing, which could affect other parts, or because silicone could emit smoke in a fire. So, although silicone is an excellent encapsulation material with high thermal conductivity and good adhesion, we can offer epoxy potting as a modified standard.

It may seem surprising, but the label design and text are considered part of the safety documentation and are strictly controlled by the certifying bodies. We regularly receive requests for custom label designs—for example, showing the customer’s own brand name and part number instead of RECOM’s standard label. Although the physical parts are identical, we must apply for a copy certificate with the new label, part number, and customer logo in order to manufacture the modified part with valid safety certification. Fortunately, we have extensive experience handling such requests and aim to make the process as fast, simple, and unbureaucratic as possible.

Once we enter the realm of semi-custom power converters, we can offer significantly more flexibility than simply tweaking specifications. This may include alternative PCB layouts to change the shape of the converter or matching the pinout to replace a competitor’s part that has become obsolete. These changes don’t have to be physical—we have also built semi-custom converters with higher-rated components to extend the operating temperature range, or harder epoxy to meet specific environmental conditions. All of these modifications are based on proven standard designs, so while the semi-custom product is tailored to meet individual requirements for form, fit, or function, it can still be produced efficiently on our standard manufacturing lines with a short time-to-market.

Semi-Custom Power Converter Examples

In 2010, a US competitor abruptly discontinued manufacturing a series of switching regulators, leaving their existing customer base ‘in the lurch.’ One customer approached us to ask whether we could modify our standard R-78 series to be pin- and function-compatible with these end-of-life products, even though the format was completely different from our existing design.

Electronic circuit boards with components

Fig. 3: The three different formats (/AC, /AL and /FC) of the R-78T series

In just 12 weeks, we released the R-78T series with three different open-frame SMD pinning options, specifically designed to be pin-compatible with these now-unavailable parts. Our ability to respond so quickly was due to the fact that we didn’t need to start from scratch—we already had extensive experience in designing and manufacturing switching regulator modules, which we used as the foundation for this semi-custom solution.
RECOM RAC20-K/X6 시리즈
Fig. 4: The semi-custom RAC20-K/X6 with IEC 62477-1 certified OVC III
More recently, we received a request for a 20W board-mount AC/DC module to be used as an auxiliary power supply in an EV charging station. Since the charging station is hard-wired to the mains supply, it falls under OVC III (Over Voltage Category III) classification and must meet additional safety requirements related to overvoltage surges, isolation ratings, and creepage and clearance distances.

We developed a semi-custom solution, the RAC20-K/X6, featuring a revised PCB layout and transformer design to comply with IEC 62477-1, OVC III requirements. It delivers reinforced isolation rated at 4kVAC for 1 minute, compared to the standard 3kVAC rating. Importantly, this was achieved without altering the module’s dimensions, pinout, or key specifications such as the wide input voltage range, extended operating temperature range, and <40mW no-load power consumption.

As is often the case with semi-custom designs, similar needs from other customers can lead to these solutions becoming standard off-the-shelf products in our portfolio.

Full-Custom Power Converter

A full-custom power converter differs from modified standard or semi-custom variants in that it is not based on an existing product. However, it still draws on proven building blocks and established production infrastructure where appropriate. Typical conditions that justify a full-custom power supply project include: no existing product can meet the technical requirements, the development costs (R&D, testing, and production) are acceptable for both parties, and the expected project volume supports the necessary investment in resources.

The typical full-custom power converter project stages are shown in Figure 5:

Project lifecycle stages

Fig. 5: Custom power converter project stages

Project Proposal

The initial request from the customer detailing the technical requirements of the custom power converter (functional specifications, performance requirements, technical standards, and physical dimensions) as well as the commercial factors (budget, expected volume, target cost, etc.)

Project Evaluation

Analysis of the technical requirements (suitability, manufacturability, resource availability, etc.). Is the project viable?

Project Plan

The project plan details the project schedule, resource allocation, and milestones that need to be achieved at each stage of the project.

Prototype

Prototypes will be built to verify compliance with the functional specifications. A change in specifications at this stage is common. RECOM understands that even when the initial custom power converter requirements are clear and well-defined, the specifications may occasionally need to be updated or modified, usually in response to market changes. This is entirely normal. As long as communication channels between the customer and the RECOM design team remain open, we aim to be as flexible as our customers.

After approval of the initial prototypes, the next step is the manufacture of pre-production prototypes (at least 50 units) to allow for statistically valid performance and stress testing.

DVT/PVT

The design verification tests (DVT) and production verification tests (PVT) are critical to the success of the project. RECOM must provide datasheets and test documentation that give the customer a high level of confidence that the custom design is fit for purpose and will perform reliably under all foreseeable operating and fault conditions.

To support this, RECOM operates an automated test lab with networked test stations for rapid testing and evaluation. This includes electrical testing, environmental testing in climate chambers, reliability testing (such as electrical and thermal stress tests, safe operating area tests, long-term soak tests, shock and vibration), and production tolerance testing.

Production and Certification Plan

As soon as the DVT testing is advanced enough to initiate a design freeze, then the production plan can be started, entailing purchasing of the necessary components from primary and second sources and ordering the custom housing, printing, and packaging. The production-ready prototypes can be sent off for agency approval (UL, IEC, EN, CB Reports, etc.).

Production

An assembly line will be set up to manufacture, test, and ship the final product to the customer.

Change Management

As mentioned previously, change is a fact of life and must be actively managed. Technical standards are typically updated every three years, and this can sometimes require modifications to the custom design to remain compliant with new regulations. Changes in the availability of key components may also require notification to, and agreement from, the customer via a Product Change Notice (PCN). Product Life Cycle (PLC) documentation is maintained throughout the lifetime of the product, up to the eventual end-of-life decision made by the customer.

Conclusion

Type Customization level Complexity Speed Added Cost
Modified Standard Product Restricted Simple Several weeks Low or no added cost
Semi Custom Flexible, but limited Medium A few months Low NRE costs, but may involve re-certification fees.
Full Custom Open Complex Several months Product-dependent, but NRE charges and new certification costs are significant
Table 1: Summary of the advantages and disadvantages of modified standard, semi-custom and full custom power converters

As can be seen by this brief introduction, a RECOM power converter can be offered as a modified standard, semi-custom, or full-custom product to the customer in several ways. Each variant has advantages and disadvantages (Table 1), so the simplest way to decide is to establish a dialog with us so we can advise and work together with you to offer the optimum solution. To facilitate this, RECOM has set up four dedicated e-mail addresses for customization requests. Someone from RECOM will then contact you to discuss your requirements in more detail.

Contact RECOM to discuss your project and for advice on how to specify your full-custom, semi-custom, or modified-standard power converter for minimum cost and fastest delivery.
  Series
1 RECOM | R-78T-1.0 Series | DC/DC, SMD, Single Output
  • Efficiency up to 95%, no need for heatsinks
  • Industry standard pin-out
  • 1.5A start-up overload capacity
  • Non-isolated regulator, very low standby current