Home Healthcare Equipment is in a Precarious Environment
We often think of industrial or professional medical environments as being ‘harsh’, with exacting cleanliness and safety standards applied to equipment; however, the operating conditions are at least well defined. In a home setting, there is a host of other variables that can affect the performance of medical power supplies and devices, and device designers are required to anticipate these in their risk assessments.
Apart from the obvious domestic temperature and humidity variations, equipment can be incorrectly used by insufficiently trained users and carers in an environment that includes children and pets. There may be spilled liquids, household dust, food debris, pet hair, and medical waste also present. The electrical supply may not have an adequate ground connection, and excessive voltage dips, spikes, and surges may be present. Moreover, radiated and conducted electromagnetic interference from other household equipment could also affect operation. Operating complex portable medical devices may be confusing and difficult for someone who is old or ill.
To address these concerns, medical electrical (ME) equipment in the home setting must meet specific safety, performance, and EMC standards. The top-level document for medical device safety and essential performance is IEC 60601-1, and this is supported by the collateral standard IEC 60601-1-11 “Requirements for medical electrical equipment and medical electrical systems used in the home healthcare environment.” Currently, the standard is dated to 2015 with amendment A1:2021.
Particular requirements of IEC 60601-1-11, additional to those in the professional healthcare environment, include the ability of mains-powered equipment to operate with 15% drops in supply voltage from nominal or 20%, if the equipment is intended for life support or resuscitation. In such cases, there must also be a mechanism for maintaining the essential performance of the equipment for a “sufficient” amount of time after the total loss of mains power as well as alarms to indicate the hazardous situation. In practice, this means that this class of equipment must have battery backup with health monitoring and alerts. If the equipment operates on a DC supply, there are also extra requirements to withstand voltage variations and 30 second dips.
Apart from the obvious domestic temperature and humidity variations, equipment can be incorrectly used by insufficiently trained users and carers in an environment that includes children and pets. There may be spilled liquids, household dust, food debris, pet hair, and medical waste also present. The electrical supply may not have an adequate ground connection, and excessive voltage dips, spikes, and surges may be present. Moreover, radiated and conducted electromagnetic interference from other household equipment could also affect operation. Operating complex portable medical devices may be confusing and difficult for someone who is old or ill.
To address these concerns, medical electrical (ME) equipment in the home setting must meet specific safety, performance, and EMC standards. The top-level document for medical device safety and essential performance is IEC 60601-1, and this is supported by the collateral standard IEC 60601-1-11 “Requirements for medical electrical equipment and medical electrical systems used in the home healthcare environment.” Currently, the standard is dated to 2015 with amendment A1:2021.
Particular requirements of IEC 60601-1-11, additional to those in the professional healthcare environment, include the ability of mains-powered equipment to operate with 15% drops in supply voltage from nominal or 20%, if the equipment is intended for life support or resuscitation. In such cases, there must also be a mechanism for maintaining the essential performance of the equipment for a “sufficient” amount of time after the total loss of mains power as well as alarms to indicate the hazardous situation. In practice, this means that this class of equipment must have battery backup with health monitoring and alerts. If the equipment operates on a DC supply, there are also extra requirements to withstand voltage variations and 30 second dips.