Finally, while ICT measurements can be performed in milliseconds, FCT procedures are typically slower, as measurements on a powered device require outputs to settle before reliable data can be taken. FCT usually takes five to ten times longer than ICT for the same product. Combining both processes in one ICT/FCT platform can create a production bottleneck. Separating the two processes allows one ICT machine to feed several FCT test fixtures in parallel, increasing test throughput and reducing delays.
Case Study: High-Current DC/DC Testing for RECOM Power
For a newly developed DC/DC product series by the Austrian company RECOM Power, the cost and time of two separate test adapters were unacceptable. A solution was needed to combine the high-speed advantage of ICT with the comprehensive quality assurance of 100% functional testing in a single test adapter. The challenge was significant: devices had up to 6A output current and input voltages up to 60V, and each PCB panel contained forty partly-finished modules requiring parallel testing with heavy-duty power supplies. High data throughput and precise timing were critical. RECOM contracted Elmatest in the Czech Republic to build a combined ICT/FCT test adapter for the Teledyne Teststation LH used by the EMS provider.
From the outset, Zdenek Martinek, application engineer at Elmatest, recognized this as a complex project. Key challenges included combining ICT/FCT in a multi-panel design, managing high relay control throughput, accelerating the FCT process, and handling high power levels without damaging sensitive probes. In close collaboration with Markus Stöger from RECOM’s R&D department, solutions were found for all issues.
Challenge 1: Integration and EMC Shielding
The first challenge was integrating ICT/FCT into the multi-panel design. Each PCB contained 40 independent circuits, fully assembled and enclosed, with some internal nodes inaccessible to the ICT pin panel. This was deliberate, as the DC/DC converters switch at high frequencies, and the metal case with its multi-layer PCB forms a six-sided Faraday cage to prevent EMI. External connections to internal high-frequency nodes could compromise
EMC shielding and cause measurement errors.
The solution was a test module on each multi-panel, providing access to all ICT nodes needed to verify proper assembly. Once the conventional ICT procedure was completed on the test module, the remaining modules required only FCT.
Fig. 3: Top and bottom images of the multi-panel PCB showing the ICT test module in the corner.
Challenge 2: Overcoming Relay Control Bottlenecks
The instructions for executing a test and measurement process are called a test vector. The input, output, and analog channel configurations are transmitted as a data burst, loaded into local on-board memory, and simultaneously activated by a timing strobe signal. This configuration remains latched until the test is completed and measurement data are returned to the CPU. Meanwhile, the next data burst can be preloaded to await the following strobe. This test methodology allows ICT to achieve fast throughput of around 4µs per vector.
Standard relay drivers in the GenRad Teststation are controlled via the PIO controller, which receives commands from the PC over an MXIbus (Figure 2). This setup was too slow for processing different FCT measurements within a single test vector using the high-speed system controller. To accelerate relay switching, a novel relay driver topology called ‘active burst’ was implemented in the RECOM test adapter.
In active burst, some relays are driven directly from the D/S outputs instead of the PIO controller. Each D/S output can be configured with nine functions, including Drive, Sense, Hold, and Collect CRC. In this case, the Drive function powered the relays directly. D/S Drive outputs are normally TTL-limited, insufficient for relay operation, but Darlington transistor current amplifier coils allowed direct control. This made relay switching virtually instantaneous and simplified coding.
Challenge 3: Accelerating FCT and Protecting Probes
Another challenge was accelerating the FCT measurements, as waiting for analog levels to settle would have been too slow. Processing power in the ICA system, using DDS and DFT techniques, enabled rapid measurement. Instead of applying a fixed load and waiting for stabilization, output loads were pulsed for milliseconds, with processed results used to derive final characteristics, reducing measurement time by up to 80%.