Material Science Advances Improve Power Supply Design and Performance

Close-up of a Printed computer mother board
It’s no secret that the quest for higher efficiency in power supplies is driving improvements in performance across a broad front. Advancements in materials science are playing a key role, in influencing power supply design and enabling the development of more efficient, compact, and reliable solutions. Here are some of the new materials that are impacting power supply design.

Wide Bandgap Semiconductors (SiC and GaN)

Of course, the first new materials that we should mention are Silicon Carbide (SiC) and Gallium Nitride (GaN), two wide bandgap semiconductors that are rapidly replacing silicon in multiple power applications. SiC and GaN power devices operate at higher temperatures and frequencies than Si, allowing for more efficient power conversion in existing designs and even allowing the use of new topologies that are not feasible with silicon devices. Power supplies utilizing these materials can be more compact and lightweight, with improved overall performance. SiC devices are gaining traction in data center high-efficiency rack-mounted designs; GaN is popular for the lower-power designs commonly found in laptop and phone chargers. There is expected to be considerable overlap between SiC and GaN in medium power applications as both materials expand their performance envelope.

Magnetic Materials

Magnetic fields are used in switching power supplies to change voltage levels, store energy, and provide galvanic isolation. New soft magnetic materials with improved magnetic properties such as high saturation flux density and low core loss are enhancing the efficiency of transformers and inductors in power supplies. These materials contribute to reduced energy losses and improved power density.

Nanocrystalline alloys are being used in the construction of magnetic cores. These materials exhibit excellent magnetic properties and reduced core losses, making them suitable for high-frequency applications in power supplies.

Dielectric Materials

New dielectric materials are improving the performance of capacitors in power supplies: enhancing energy storage, reducing losses, improving efficiency, and ensuring reliable operation under various operating conditions. These materials can withstand higher voltages and frequencies, contributing to increased power density and reliability.

Advancements in polymer capacitor materials, such as conductive polymers, have led to capacitors with improved conductivity, lower equivalent series resistance (ESR), and longer lifespans. Polymer capacitors are increasingly used in power supply applications for their enhanced performance.

Insulating Materials

These materials play a critical role in the insulation systems of transformers, capacitors, and other components. Improvements in this area reduce losses, increase reliability, and enable more compact and efficient designs by improving thermal performance.

High performance ceramic insulators such as aluminum nitride (AlN) and silicon nitride (Si3N4), provide excellent thermal conductivity and electrical insulation properties.

Advanced Conductive Materials

The use of high conductivity metals and alloys, including copper and aluminum alloys with improved conductivity, contributes to reduced resistive losses in power supply components such as conductors and connectors.

Flexible and Stretchable Materials

The development of flexible substrates and stretchable materials is enabling the design of flexible and conformable power supplies. These materials are suitable for applications where space constraints and unconventional form factors are critical.

3D Printing Materials

3D printing technologies allow the use of a variety of materials in power supply manufacturing. Additive manufacturing enables the creation of complex and customized components, leading to improved design flexibility and rapid prototyping.

Thermal Interface Materials

The effective removal of heat is essential for maintaining the reliability, efficiency, and longevity of electronic components in a power supply. Thermal interface materials are placed between a heat-generating device such as a power transistor and a heat-dissipating device such as a heat sink. They include thermal adhesives, pads, pastes, and gaskets, and are crucial for effective heat dissipation. New materials such as thermal gels with high thermal conductivity and improved thermal resistance properties help in managing the heat generated by power electronic components, enhancing overall reliability and performance.

Looking further ahead, graphene and carbon nanotubes are being explored for thermal management applications in power supplies. These materials offer excellent thermal conductivity, making them suitable for heat dissipation solutions in high power density environments.

Eco-friendly Materials

Increasing emphasis on sustainability is driving the use of eco-friendly materials in power supply design. This includes materials with low environmental impact, recyclable components, and adherence to RoHS (Restriction of Hazardous Substances) standards.

Advanced Nanomaterials

Nanomaterials such as nanocomposites are being explored for their unique electrical, thermal, and mechanical properties. Incorporating nanomaterials in various components of power supplies can enhance their performance and efficiency.

Printable Electronics Materials

In the realm of flexible and printed electronics, printable conductive inks based on novel materials are being developed. These inks enable the fabrication of printed circuitry and components, providing new possibilities for power supply design and manufacturing.

RECOM Takes Advantage of Material Science Advances

RECOM products take full advantage of upgrades as these material science advancements meet our demanding quality standards and make their way into volume production. Many of the improvements in this area might not be obvious to the customer, manifesting themselves as improvements in efficiency, an extended temperature range, or an increase in reliability.

The new RKK, for example, is an upgrade to the popular existing RKE/RFMM series, a 1W unregulated, isolated, SIP-7 DC/DC. The RKK boasts improved magnetics with a planar transformer and now has lower EMI, operation to 105°C with no derating, longer lifetime figure, and higher efficiency which is maintained to light loads. Elimination of potting saves cost and weight, nearly halving to just 1.7g, adding to its ‘green’ credentials. An additional new series, RYK, has a fully linear-regulated output with similar enhancements.

Conclusion

Ongoing research and innovations in materials science continue to shape the evolution of power supply technologies. Advances are occurring on a broad front, benefiting power supplies with improved semiconductor materials, dielectrics, insulators, sustainability, and more.

Incorporating these advanced materials into power supply design contributes to improvements in efficiency, reliability, miniaturization, and sustainability. RECOM designers are constantly evaluating new components that employ new materials and adding them to our designs as appropriate.
Applications
  Series
1 DC/DC, 1 W, Single Output, THT RKK Series
Focus
  • Low cost
  • 1:1 Input voltage range
  • Efficiency up to 82%
  • 4kVDC/1 second isolation
2 DC/DC, 1 W, Single Output, THT RYK Series
Focus
  • Low cost
  • 1:1 Input voltage range
  • Efficiency up to 81%
  • 4kVDC/1 second isolation