Converting one DC voltage to another in an electronic circuit has a history that demonstrates over fifty years of increasing sophistication — modern designs having incredibly high-power densities along with corresponding advances in efficiency to keep the power dissipation low. RECOM’s current designs include many innovations that apply design techniques from high-power power supplies to benefit low-wattage converters in the smallest packages.
The first DC/DC conversion solutions were all low-noise linear designs that were simple to use but had two major drawbacks. First, the output voltage must always be lower than the input voltage; however, a linear regulator is very inefficient and dissipates a substantial proportion of the supplied power as heat. Second, depending on the voltage difference between input and output, linear regulator efficiencies can be 60% or lower.
The invention of the switching DC/DC converter solved both problems but required a more complex design methodology. In contrast to linear designs, switching converters exploit the energy-storing properties of inductive and capacitive components to transfer power in discrete packets. The pulses of power are stored either in an inductor's magnetic field or in a capacitor's electric field.
The first DC/DC conversion solutions were all low-noise linear designs that were simple to use but had two major drawbacks. First, the output voltage must always be lower than the input voltage; however, a linear regulator is very inefficient and dissipates a substantial proportion of the supplied power as heat. Second, depending on the voltage difference between input and output, linear regulator efficiencies can be 60% or lower.
The invention of the switching DC/DC converter solved both problems but required a more complex design methodology. In contrast to linear designs, switching converters exploit the energy-storing properties of inductive and capacitive components to transfer power in discrete packets. The pulses of power are stored either in an inductor's magnetic field or in a capacitor's electric field.