Rutronik Racing powered by RECOM

Rutronik Racing fueled by RECOM
RECOM is honored to be the number one power supply brand for Rutronik, an electronics distributor of high-scale and complex electronic components. RECOM has partnered with the ADAC GT MASTERS team Rutronik Racing since 2018. In 2023, Rutronik Racing Team changed to another motorsport class—GTWC Europe Endurance Cup and Rutronik Racing continues to be supported by RECOM.

The Rutronik Racing Team is moving their manufacturer from Audi Sport to Porsche Motorsport, which started this new trajectory into the team’s debut in the GT World Challenge Europe Endurance Cup. The racing team will compete for the second time in the 24h program at the Nürburgring as a factory team with Porsche Motorsport. The Rutronik Racing Team is able to create a strategic international footprint by partaking in these races. The racing team’s emphasis on international cooperation gives them a chance to improve ABU-related communication on a worldwide scale. The GT World Challenge Endurance Cup calendar offers an international focus providing Rutronik partners the chance to interact with customers throughout Europe.

Alongside this racing partnership, RECOM is proud to support Formula Student teams, future engineers, and the next generation of racing. RECOM provides DC/DC converters for IGBT and SiC MOSFET applications that use power-sharing technology and can run with constant power to support Formula Students.
Applications