Bitte beachten Sie, dass dieser Abschnitt nur als Referenz gedacht ist. Produktbeschreibungen und Spezifikationen können sich seit der Veröffentlichung dieser Publikationen geändert haben.
Electric vehicles, and e-mobility, in general, are the future of transportation in a world that needs to reduce its carbon footprint. To make the use of battery powered...
Over the years, RECOM has expanded its portfolio of DC/DC converters for the railway industry from 3W up to 240W and is now able to offer one of the market’s broadest...
Today’s medical applications have strict regulatory requirements in both hospital and non-hospital environments. We specifically designed our cost-effective DC/DC and AC/DC...
Over the years, RECOM has expanded its portfolio of DC/DC converters for the railway industry from 3W up to 240W and is now able to offer one of the market’s broadest...
To meet the emerging demands of smart building applications, RECOM extends its existing low-power RAC series with new household certified AC/DC converters more cost efficient.
RECOM’s constant current (CC) and constant voltage (CV) low profile LED drivers have been designed for cost-sensitive applications. Screw terminal or wired versions make them...
RECOM’s energy-efficient AC/DC and DC/DC converters live up to the Industry 4.0 and IoT challenges and offer high efficiency at both light load and full load at affordable...