Powering 5G Infrastructure

Drone circuit board with 5G symbol
5G base stations are set to grow exponentially in number along with associated energy consumption, so providing power efficiently is important. This article discusses the subject and suggests some power module solutions that offer high power density and reliable performance in the base station environment.

Rollout of 5G is now well underway, with coverage on track for one third of the world’s population by 2025, according to the GSMA [1]. Major cell phone manufacturers have launched 5G-enabled phones, which will please those wanting to stream data and videos at up to the theoretical 50Gb/s maximum speed, and worldwide 5G subscriptions are forecast to reach 1.3bn by 2023, according to Statista [2].

However, 5G is much more than faster smartphones – it underpins the technology behind artificial intelligence, cloud computing, autonomous vehicles, the internet of things (IoT), smart cities and industry, and probably more yet-undreamed of applications. As a result, investment in new 5G infrastructure will be high, and network operators will be looking for the quickest possible return on what is projected by Statista to be 1.4 trillion dollars’ telecom services spent in 2021 alone.

5G may eventually work at over 70GHz

5G infrastructure is not simply an upgrade to 4G; by its nature, at peak performance, 5G uses higher frequencies, and coverage is less, so more cells are required. Three bands are available: low, mid, and high, with the majority of installations using mid-band at 2.5 – 3.7GHz, at speeds up to 900Mb/s. The low band uses similar frequencies to 4G with similar range and coverage, so it offers little extra benefit but may be used in low traffic areas to achieve basic but wide coverage quickly. High band, eventually working at over 70GHz, yields the fastest data rates, but coverage is very limited, perhaps 1.5km, so it is preferred for public areas such as arenas, markets, and conference centers. Traffic in these locations can be high, but base stations can be small and distributed around a restricted area with ‘beamforming’ techniques to provide good coverage.

Cells therefore fall into coverage categories ‘metro’, ’micro’, ‘pico’, and ‘femto’ with reducing power outputs and range, from a Multiple Input Multiple Output (MIMO) metro cell transmitting over 100W to a femto cell operating at milliwatt levels. The term ‘small cell’ is also used for the three smallest categories together. With the increased throughput and number of base stations, energy consumption is set to rise overall, with some reports predicting a doubling compared with 4G. As energy is a major cost to network operators (5% to 6% with 4G according to MTN consulting [3]), there is extreme pressure to increase efficiency of all elements in base station electronics.

RF PA stages are not very efficient

One particularly inefficient stage in a base station is the RF power amplifier (Figure 1), which traditionally has use LDMOS devices which can generate kW up to a few GHz. However, in pursuit of better efficiency at the higher frequencies of 5G, gallium nitride (GaN) devices which suit the lower power/higher volume small-cell installations are increasingly used. LDMOS is typically powered from 26-32V DC rails while GaN uses 50-60V. Efficiency of a RF PA is still not high, at around 60% maximum, so every watt saved in generating the power rails from a battery backed system supply, perhaps at 48V, is valuable.

Schematic of RPA150E-48SEW/P

Fig. 1: Typical 5G base station RF stage with envelope tracking for maximum efficiency (only one channel of a MIMO shown)
The RPA150E series is a suitable DC/DC converter for a 5G power amplifier stage [4]. It is galvanically isolated, so the input voltage can be a typical telecom -48VDC or -24VDC supply while the output is positive with respect to ground (Figure 1). The RPA150E can deliver 150W continuously and up to 200W peak power to supply the output RF power amplifiers, and the nominal output voltage can be trimmed ±20% to supply the optimum supply voltage for maximum efficiency. The 1/8th sized brick format has a very small footprint for the rated power, and the baseplate cooling allows high temperature operation without derating.

An important feature of DC/DC converters in 5G applications is to have low quiescent power draw and the ability to be set into a low-power shut down mode. Unlike 4G, which continually transmits system information and synchronization/reference signals even with no user traffic, 5G has defined advanced ‘sleep’ modes (ASMs) that are used to minimize average power consumption. Power savings are traded against latency but the gains of around 50% are extremely attractive. Having low-power shutdown features in the system DC/DC converters is therefore important. The RPA150E is also ideal for use with battery-powered supplies, having a conversion efficiency of >91% and a standby consumption of only 3mA.

‘Envelope tracking’ is increasingly used to vary the RF PA supply voltage to match the amplitude of the modulating signal to increase system efficiency, but this must operate at MHz rates, so any dynamic output voltage adjustment function of a DC/DC converter cannot be fast enough. An external envelope tracking circuit using GaN transistors for high speed dynamic tracking can be easily implemented to pulse the drain current to the RF amplifier (Figure 1).

Base stations have a range of digital and analoge electronics needing power

Other electronics in a base station is a mixture of low noise analog signalling and digital processing, using familiar components such as CPUs, FPGAs, SoC devices, ADCs, DACs, and more. These components require voltage rails that might range from +5V for a DAC down to sub 1V for a processor or FPGA and typically employ non-isolated point of load converters (PoLs) or ‘power modules’ to provide an accurate, low-noise voltage right at the load. Input voltage to the PoL may be a system 48V or more likely, a regulated ‘intermediate bus’ at typically 12V.

Products from RECOM's RPX and RPL and RPM series

Fig. 2: The RECOM RPX series power module is tiny but rated at up to 4A output
Isolated DC/DC converters and power modules in 5G base stations often operate in a difficult environment with potential temperature extremes, transients from lightning strikes and other equipment, high RF fields and all in the smallest enclosure at the lowest acquisition cost. Reliability is paramount to avoid unnecessary maintenance expenses and electrical efficiency must be high to keep energy costs low and the burden of heat generation on other components minimized.

Non-isolated power modules are also featured in the RECOM portfolio with ultra-compact, high efficiency parts using the company’s ‘3D Power Packaging®’ technologies.

The RECOM RPX-1.0 and RPX-1.5 series have a minimal 3 x 5mm footprint in a low-profile QFN package. The part uses flip-chip technology for extremely high power density, with 1A or 1.5A rated output, adjustable from 0.8-30V, for input voltages from 4-36V. With only a slightly larger footprint (4 x 4.5mm), the RPX-2.5 offers 2.5A output current. If component height is not so restricted, the RPX-4.0 offers 4A output current in a compact 5 x 5.5 x 4.1mm package. All of these converters are complete with integrated inductors and full protection (UVLO, SCP, OCP, OTP), requiring only output voltage setting resistors and input and output capacitors to form complete power supplies

At higher output currents, up to 6A, the RPM series is suitable, with an input voltage range of 4-15V and output adjustable from 0.9-6V. Efficiency peaks at 99%, allowing the part to operate reliably in ambient temperatures of up to 90°C without forced air cooling.

Input VDC vs. Output Current Graph
Fig. 3: Sub-miniature LGA power module ranges available from RECOM
If board space is very restricted, the RPL-3.0 series is ideal. The input voltage range is 4-18 VDC, and the output voltage can be adjusted to anywhere between 0.8 VDC and 5.2 VDC. The maximum continuous output current is 3A - impressive for a converter which is only 3 x 3 x 1.45mm small.

All the parts mentioned include comprehensive protection and monitoring, including a shutdown control for energy saving when a 5G base station is in a sleep state. Figure 3 summarizes the power ranges available.

5G promises huge improvements in communications performance, opening up many new and exciting applications. System designers however are aware that energy consumption must be minimized for 5G to be viable and for minimum environmental impact. Use of reliable power converters with high efficiency and power density and which are rated for the difficult base station environment are key enablers to achieve this. RECOM can support the application with a wide range of suitable converters.

References

[1] GSMA: Global System for Mobile Communications: http://www.gsma.com
[2] http://www.statista.com/topics/3447/5g
[3] http://www.mtnconsulting.biz/product/operators-facing-power-cost-crunch/
[4] https://recom-power.com/rec-s-RPA150E-EW.html
용도
  Series
1 DC/DC, 150.0 W, Single Output, THT RPA150E-EW Series
Focus
  • 150W industrial grade isolated DC-DC
  • Compact, industry standard 1/8th brick format
  • 6:1 input voltage range (9-60 VDC)
  • 3kVDC Isolation
2 DC/DC, 15.0 W, Single Output, SMD (pinless) RPL-3.0 Series
Focus
  • Wide input range (4 - 18V)
  • Low profile 1.45mm
  • Small footprint 3x3mm
  • Adjustable output 0.8 to 5.2V
3 DC/DC, 15.0 W, Single Output RPL-3.0-EVM-1 Series
Focus
  • Evaluation platform for RPL-3.0 Buck Regulator Module
  • Thermal design considerations included
  • EMI Class A filter
  • Easy evaluation of output voltage selection, control, power good and sensing functions
4 DC/DC, Single Output, SMD (pinless) RPM-6.0 Series
Focus
  • High power density (L*W*H = 12.19*12.19*3.75)
  • Wide operating temperature -40°C to +90°C at full load
  • Efficiency up to 99%, no need for heatsinks
  • 6-sided shielding
5 DC/DC, 5.0 W, Single Output, SMD (pinless) RPX-1.0 Series
Focus
  • Buck regulator power module with integrated shielded inductor
  • 36VDC input voltage, 1A output current
  • SCP, OCP, OTP, and UVLO protection
  • 3.0 x 5.0mm low profile QFN package
6 DC/DC, 7.5 W, Single Output, SMD (pinless) RPX-1.5 Series
Focus
  • Buck regulator power module with integrated shielded inductor
  • 36VDC input voltage, 1.5A output current
  • SCP, OCP, OTP, and UVLO protection
  • 3.0 x 5.0mm low profile QFN package
7 DC/DC, 12.5 W, Single Output, SMD (pinless) RPX-2.5 Series
Focus
  • Buck regulator power module with integrated shielded inductor
  • 28V maximum input voltage
  • 2.5A maximum output current
  • SCP, OCP, OTP, OVP and UVLO protection
8 DC/DC, 20.0 W, Single Output, SMD (pinless) RPX-4.0 Series
Focus
  • Buck regulator power module with integrated shielded inductor
  • 36VDC input voltage, 4A output current
  • Programmable output voltage: 1 to 7V
  • Ultra-high power density: 5.0 x 5.5mm QFN footprint
9 DC/DC, 20.0 W, Single Output RPX-4.0-EVM-1 Series
Focus
  • Evaluation platform for RPX-4.0 buck regulator module
  • Thermal design considerations included
  • EMI class B filter
  • Easy evaluation of output voltage selection, control, and sensing functions
10 DC/DC, Single Output RPM-6.0-EVM-1 Series
  • Evaluation platform for RPM-6.0 buck regulator modules
  • Thermal design considerations included
  • EMI Class B filter
  • Easy evaluation of trimming, sequencing, soft start, enable and sensing functions
11 DC/DC, 5.0 W, Single Output RPX-1.0-EVM-1 Series
  • Evaluation platform for RPX-1.0 buck regulator module
  • Thermal design considerations included
  • EMI class B filter
  • Easy evaluation of output voltage selection, control, and sensing functions
12 DC/DC, 7.5 W, Single Output RPX-1.5-EVM-1 Series
  • Evaluation platform for RPX-1.5 buck regulator module
  • Thermal design considerations included
  • EMI class B filter
  • Easy evaluation of output voltage selection, control, and sensing functions
13 DC/DC, 12.5 W, Single Output RPX-2.5-EVM-1 Series
  • Evaluation platform for RPX-2.5 buck regulator module
  • Thermal design considerations included
  • EMI Class B filter
  • Easy evaluation of output voltage selection, control and sensing functions