GaN Gate Drive Considerations - lntroduction
Gallium Nitride (GaN) semiconductors are High Electron Mobility Transistor (HEMT) devices—a class of transistors known for their near-ideal switching characteristics. In a HEMT, electrons move within the crystal structure as a two-dimensional electron gas with extremely high mobility, resulting in a device with excellent conductivity and low RDS(ON). The unique properties of GaN increase the breakdown voltage, allowing the internal transistor layers to be made thinner and more closely spaced. This enhances switching speed and lowers gate capacitance.
Enhancement-mode GaN transistors (E-HEMTs) feature a depletion zone beneath the gate that blocks electron flow until a positive gate voltage is applied relative to the source pin. Because this depletion zone is extremely thin, only a small amount of charge is required to turn the device on or off, enabling switching speeds in the MHz range without significant switching losses.
Fig. 1: Diagrammatic layout of an Enhancement Mode GaN Transistor in the OFF and ON modes
The extreme thinness of the gate isolation layer means that high gate-source voltages can cause internal flashover, despite the material’s high breakdown voltage rating. A GaN E-HEMT typically reaches full enhancement at 7V but can be damaged if VGS exceeds ±10V — significantly lower than the gate voltages commonly used in IGBT or SiC
gate drivers. Due to the very fast rise and fall times of the low-capacitance gate channel, any excessive inductance in the external gate drive may cause voltage spikes or ringing, potentially exceeding these voltage limits. A 6V gate drive voltage provides a good balance between efficiency and safe operation.
IGBT and SiC gate drive circuits often use a negative gate voltage during turn-off to accelerate charge extraction from the gate capacitance, reducing switch-off time. In contrast, GaN transistors have such low gate capacitance that a negative gate voltage is unnecessary. A 0V gate voltage will reliably turn off the HEMT in nanoseconds. Only in cases of excessive layout inductance would a negative gate drive offer protection against unintended turn-on from ringing. However, since HEMTs lack a body diode like MOSFETs and conduct symmetrically, a negative gate voltage increases reverse conduction losses. A single-ended 6V–0V gate drive is ideal. Figure 2 illustrates typical gate driver voltages used for GaN, along with those for IGBT and first- and second-generation SiC devices.
Fig. 2: Typical Gate Driver supply voltages for IGBT, SiC and GaN drivers